![]() |
MCUXpresso SDK API Reference Manual
Rev 2.14.0
NXP Semiconductors
|
Data Structures | |
| struct | boot_cmd_t |
| Boot command definition. More... | |
| struct | boot_hdr1_t |
| Definition for boot image file header chunk 1. More... | |
| struct | boot_hdr2_t |
| Definition for boot image file header chunk 2. More... | |
| struct | crc32_data_t |
| State information for the CRC32 algorithm. More... | |
| struct | ldr_Context_t |
| Loader context definition. More... | |
| struct | mem_region_t |
| Memory region information table. More... | |
| struct | mem_attribute_t |
| Memory Attribute Structure. More... | |
| struct | mem_context_t |
| Memory context structure. More... | |
| struct | api_memory_region_interface_t |
| Memory region interface structure. More... | |
| struct | api_memory_map_entry_t |
| Memory entry data structure. More... | |
| struct | api_core_context_t |
| The API context structure. More... | |
| struct | sb3_data_range_header_t |
| section data range structure More... | |
| struct | sb3_section_header_t |
| sb3 DATA section header format More... | |
| struct | kb_region_t |
| Memory region definition. More... | |
| struct | ldr_Context_v3_t |
| Loader context definition. More... | |
Macros | |
| #define | SB_FILE_MAJOR_VERSION (3) |
| Determines the version of SB loader implementation (1: sb1.0; 2: sb2.0; 3.1: sb3.1) | |
| #define | kStatusGroup_SBLoader (101U) |
| Bootloader status group numbers. | |
| #define | RAM_REGION_COUNT (2U) |
| Contiguous RAM region count. | |
| #define | FLASH_REGION_COUNT (1U) |
| Contiguous FLASH region count. | |
| #define | FFR_REGION_COUNT (1U) |
| Contiguous FFR region count. | |
| #define | MEM_INTERFACE_COUNT (4U) |
| Memory Interface count. | |
| #define | FLEXSPINOR_REGION_COUNT (1U) |
| Contiguous FLEXSPINOR meomry count. | |
| #define | BYTES_PER_CHUNK 16 |
| Defines the number of bytes in a cipher block (chunk). More... | |
| #define | BOOT_SIGNATURE 0x504d5453 |
| Boot image signature in 32-bit little-endian format "PMTS". | |
| #define | BOOT_SIGNATURE2 0x6c746773 |
| Boot image signature in 32-bit little-endian format "ltgs". | |
| #define | FFLG_DISPLAY_PROGRESS 0x0001 |
| These define file header flags. | |
| #define | SFLG_SECTION_BOOTABLE 0x0001 |
| These define section header flags. | |
| #define | CFLG_LAST_TAG 0x01 |
| These define boot command flags. | |
| #define | ROM_ERASE_ALL_MASK 0x01 |
| ROM_ERASE_CMD flags. | |
| #define | ROM_JUMP_SP_MASK 0x02 |
| ROM_JUMP_CMD flags. | |
| #define | ROM_MEM_DEVICE_ID_SHIFT 0x8 |
| Memory device id shift at sb command flags. | |
| #define | ROM_MEM_DEVICE_ID_MASK 0xff00 |
| Memory device id mask. | |
| #define | ROM_MEM_GROUP_ID_SHIFT 0x4 |
| Memory group id shift at sb command flags. | |
| #define | ROM_MEM_GROUP_ID_MASK 0xf0 |
| Memory group id flags mask. | |
| #define | ROM_PROG_8BYTE_MASK 0x01 |
| ROM_PROG_CMD flags. | |
| #define | ROM_NOP_CMD 0x00 |
| These define the boot command tags. | |
| #define | ROM_BOOT_SECTION_ID 1 |
| Plugin return codes. | |
| #define | SB3_BYTES_PER_CHUNK 16 |
| Defines the number of bytes in a cipher block (chunk). More... | |
| #define | SB3_DATA_RANGE_HEADER_FLAGS_ERASE_MASK (0x1u) |
| bit 0 | |
| #define | SB3_DATA_RANGE_HEADER_FLAGS_LOAD_MASK (0x2u) |
| bit 1 | |
| #define | SBLOADER_V3_CMD_SET_ALL |
| The all of the allowed command. | |
| #define | SBLOADER_V3_CMD_SET_IN_ISP_MODE |
| The allowed command set in ISP mode. | |
| #define | SBLOADER_V3_CMD_SET_IN_REC_MODE |
| The allowed command set in recovery mode. | |
Typedefs | |
| typedef status_t(* | pLdrFnc_t )(ldr_Context_t *context) |
| Function pointer definition for all loader action functions. More... | |
| typedef status_t(* | pJumpFnc_t )(uint32_t parameter) |
| Jump command function pointer definition. More... | |
| typedef status_t(* | pCallFnc_t )(uint32_t parameter, uint32_t *func) |
| Call command function pointer definition. More... | |
| typedef status_t(* | pLdrFnc_v3_t )(ldr_Context_v3_t *content) |
| Function pointer definition for all loader action functions. More... | |
Enumerations | |
| enum | |
| SB loader status codes. More... | |
| enum | section_type_t { kSectionNone = 0 } |
| sb3 section definitions More... | |
| enum | sb3_cmd_t |
| loader command enum | |
| enum | kb_operation_t { kRomAuthenticateImage = 1, kRomLoadImage = 2 } |
| Details of the operation to be performed by the ROM. More... | |
Functions | |
| status_t | Sbloader_Init (api_core_context_t *ctx) |
| Perform the Sbloader runtime environment initialization This API is used for initializing the sbloader state machine before calling the api_sbloader_pump. More... | |
| status_t | Sbloader_Pump (api_core_context_t *ctx, uint8_t *data, uint32_t length) |
| Handle the SB data stream This API is used for handling the secure binary(SB3.1 format) data stream, which is used for image update, lifecycle advancing, etc. More... | |
| status_t | Sbloader_Finalize (api_core_context_t *ctx) |
| Finish the sbloader handling The API is used for finalizing the sbloader operations. More... | |
| struct boot_cmd_t |
| struct boot_hdr1_t |
| struct boot_hdr2_t |
Data Fields | |
| uint32_t | bootOffset |
| chunk offset to the first boot section | |
| uint32_t | bootSectID |
| section ID of the first boot section | |
| uint16_t | keyCount |
| number of keys in the key dictionary | |
| uint16_t | keyOffset |
| chunk offset to the key dictionary | |
| uint16_t | hdrChunks |
| number of chunks in the header | |
| uint16_t | sectCount |
| number of sections in the image | |
| struct crc32_data_t |
Data Fields | |
| uint32_t | currentCrc |
| Current CRC value. More... | |
| uint32_t | byteCountCrc |
| Number of bytes processed. More... | |
| uint32_t crc32_data_t::currentCrc |
| uint32_t crc32_data_t::byteCountCrc |
| struct _ldr_Context |
Provides forward reference to the loader context definition.
Data Fields | |
| pLdrFnc_t | Action |
| pointer to loader action function | |
| uint32_t | fileChunks |
| chunks remaining in file | |
| uint32_t | sectChunks |
| chunks remaining in section | |
| uint32_t | bootSectChunks |
| number of chunks we need to complete the boot section | |
| uint32_t | receivedChunks |
| number of chunks we need to complete the boot section | |
| uint16_t | fileFlags |
| file header flags | |
| uint16_t | keyCount |
| number of keys in the key dictionary | |
| uint32_t | objectID |
| ID of the current boot section or image. | |
| crc32_data_t | crc32 |
| crc calculated over load command payload | |
| uint8_t * | src |
| source buffer address | |
| chunk_t | initVector |
| decryption initialization vector | |
| chunk_t | dek |
| chunk size DEK if the image is encrypted | |
| chunk_t | scratchPad |
| chunk size scratch pad area | |
| boot_cmd_t | bootCmd |
| current boot command | |
| uint32_t | skipCount |
| Number of chunks to skip. | |
| bool | skipToEnd |
| true if skipping to end of file | |
| uint32_t | offsetSignatureBytes |
| offset to signagure block header in bytesn | |
| struct mem_region_t |
| struct mem_attribute_t |
| struct mem_context_t |
| struct api_memory_region_interface_t |
| struct api_memory_map_entry_t |
| struct api_core_context_t |
| struct sb3_data_range_header_t |
| struct sb3_section_header_t |
| struct kb_region_t |
| struct _ldr_Context_v3 |
Provides forward reference to the loader context definition.
Data Fields | |
| pLdrFnc_v3_t | Action |
| pointer to loader action function | |
| uint32_t | block_size |
| size of each block in bytes | |
| uint32_t | block_data_size |
| data size in bytes (NBOOT_SB3_CHUNK_SIZE_IN_BYTES) | |
| uint32_t | block_data_total |
| data max size in bytes (block_size * data_size | |
| uint32_t | block_buffer_size |
| block0 and block size | |
| uint32_t | processedBlocks |
| will be used for both block0 and blockx | |
| bool | in_data_block |
| data block offset in a block. More... | |
| bool | in_data_section |
| in progress of handling a data section within a data block | |
| bool | in_data_range |
| in progress of handling a data range within a data section | |
| uint32_t | commandSet |
| support command set during sb file handling | |
| uint8_t | data_buffer [SB3_DATA_BUFFER_SIZE_IN_BYTE] |
| temporary data buffer | |
| kb_options_t | fromAPI |
| options from ROM API | |
| bool ldr_Context_v3_t::in_data_block |
in progress of handling a data block within a block
| #define BYTES_PER_CHUNK 16 |
This is dictated by the encryption algorithm.
| #define SB3_BYTES_PER_CHUNK 16 |
This is dictated by the encryption algorithm.
| typedef status_t(* pLdrFnc_t)(ldr_Context_t *context) |
| typedef status_t(* pJumpFnc_t)(uint32_t parameter) |
| typedef status_t(* pCallFnc_t)(uint32_t parameter, uint32_t *func) |
| typedef status_t(* pLdrFnc_v3_t)(ldr_Context_v3_t *content) |
| anonymous enum |
| enum section_type_t |
| enum kb_operation_t |
The kRomAuthenticateImage operation requires the entire signed image to be available to the application.
| Enumerator | |
|---|---|
| kRomAuthenticateImage |
Authenticate a signed image. |
| kRomLoadImage |
Load SB file. |
| status_t Sbloader_Init | ( | api_core_context_t * | ctx | ) |
This API should be called after the iap_api_init API.
| ctx | Pointer to IAP API core context structure. |
| kStatus_Success | Api was executed succesfuly. |
| status_t Sbloader_Pump | ( | api_core_context_t * | ctx, |
| uint8_t * | data, | ||
| uint32_t | length | ||
| ) |
This API should be called after the iap_api_init and api_sbloader_init APIs.
| ctx | Pointer to IAP API core context structure. |
| data | Pointer to source data that is the sb file buffer data. |
| length | The size of the process buffer data. |
| kStatus_Success | Api was executed succesfuly. |
| kStatus_InvalidArgument | An invalid argument is provided. |
| kStatus_Fail | API execution failed. |
| status_t Sbloader_Finalize | ( | api_core_context_t * | ctx | ) |
| ctx | Pointer to IAP API core context structure. |
| kStatus_Success | Api was executed succesfuly. |